Feedback_Velocity_Error_Limit

Index.Sub  2230.1EH
Data Type Unsigned32
Access Read/Write
PDO Mappable No
Unit

0.01 rpm

Range

Unsigned32
Default Value 1000
Store Supported Yes
Description This value is used for Closed Loop feature and defines the maximum allowed displacement between motor reference velocity and motor actual velocity detected by Feedback Sensor.

Notes

--